Everything

Comparator

Below is a list of API functions output by the Code Generator for comparator use.

 

Table 3.28 API Functions: [Comparator]

API Function Name

Function

R_COMP_Create

Performs initialization necessary to control the comparator.

R_COMP_Create_UserInit

Performs user-defined initialization relating to the comparator.

r_compn_interrupt

Performs processing in response to the comparator interrupt INTCMPn.

R_COMPn_Start

Begins comparison of reference input voltage and analog input voltage.

R_COMPn_Stop

Stops comparison of reference input voltage and analog input voltage.

R_COMP_Reset

Reset the comparator.

R_COMP_Set_PowerOff

Halts the clock supplied to the comparator.