Everything

Temperature sensor

Below is a list of API functions output by the Code Generator for temperature sensor use.

 

Table 3.24 API Functions: [Temperature Sensor]

API Function Name

Function

R_TMPS_Create

Performs initialization necessary to control the temperature sensor.

R_TMPS_Create_UserInit

Performs user-defined initialization relating to the temperature sensor.

R_TMPS_Start

Starts measurement of the temperature that uses the temperature sen sor.

R_TMPS_Stop

Ends measurement of the temperature that uses the temperature sensor.

R_TMPS_Reset

Reset the temperature sensor.

R_TMPS_Set_PowerOff

Halts the clock supplied to the temperature sensor.