Data transfer controller
Below is a list of API functions output by the Code Generator for Data transfer controller use.
Table 3.38 API Functions: [Data transfer controller]
API Function Name |
Function |
Performs initialization necessary to control the Data transfer controller. | |
Performs user-defined initialization relating to the Data transfer controller. | |
Enables operation of the Data transfer controller. | |
Disables operation of the Data transfer controller. | |
Halts the clock supplied to the Data transfer controller. | |
Enables operation of the Data transfer controller. | |
Disables operation of the Data transfer controller. |