SPI interface
Below is a list of API functions output by the Code Generator for SPI interface use.
Table 3.45 API Functions: [SPI Interface]
API Function Name |
Function |
Performs initialization necessary to control the SPI interface. | |
Performs user-defined initialization relating to the SPI interface. | |
Starts SPI data transmission. | |
Starts SPI data reception. | |
Performs initialization necessary to control the SPI interface. | |
Performs user-defined initialization relating to the SPI interface. | |
Starts SPI data transmission. | |
Starts SPI data reception. |