Everything

Clock output/buzzer output controller

Below is a list of API functions output by the Code Generator for clock output/buzzer output controller use.

 

Table 3.19 API Functions: [Clock Output/Buzzer Output Controller]

API Function Name

Function

R_PCLBUZn_Create

Performs initialization necessary to control the clock/buzzer output controller.

R_PCLBUZn_Create_UserInit

Performs user-defined initialization relating to the clock/buzzer output controller.

R_PCLBUZn_Start

Starts clock/buzzer output.

R_PCLBUZn_Stop

Ends clock/buzzer output.

R_PCLBUZn_Set_PowerOff

Halts the clock supplied to the clock/buzzer output controller.