Everything

Common

Below is a list of API functions output by the Code Generator for common use.

 

Table 3.1   API Functions: [Common]

API Function Name

Function

hdwinit

Performs initialization necessary to control the various hardwares.

This API is automatically called from the startup routine of Renesas-made compiler.

R_Systeminit

Performs initialization necessary to control the various peripheral functions.

main

This is a main function.

R_MAIN_UserserInit

Performs user-defined initialization.